11/24/2013 6:34 PM | |
Posts: 6 Rating:
|
hi, does someone tried this example aplication?(https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objid=56969417&nodeid4=20229695&caller=view&switchLang;56969417;2.x=34&switchLang;56969417;2.y=4&lang=de&siteid=cseus&aktprim=4&objaction=csopen&extranet=standard&viewreg=WW) I wanted make own application and i have trouble with compiling code from matlab. i have installed matlab 2013a with necessary plugins ( MATLAB Coder V2.3, Simulink Coder V8.3, Embedded Coder V6.3), WinAC ODK V4.2 SP1, WinAC Target ( installed m-file in matlab), Microsoft Visual Studio 2010 Professional Win7 32bit like in manual https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objid=56969417&nodeid4=20229695&caller=view&switchLang;56969417;2.x=34&switchLang;56969417;2.y=4&lang=de&siteid=cseus&aktprim=4&objaction=csopen&extranet=standard&viewreg=WW. I made my own model in Simulink similary like example from Siemens, and i can't made build model by WinAC target (.dll). Building by WinAC Target start good and crash with the one file: ert_main.cpp(112) : error C3861: 'rtERTExtModeParseArgs': identifier not found. Full crash code in file Matlab error. If anyone can help me I would be very grateful
Attachmentmatlab_error.zip (379 Downloads) |
11/25/2013 8:38 AM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating:
|
Thread closed, because question is already published in the following thread WinAC Target with Matlab/Simulink Best regards O_Moderator |
Follow us on