9/20/2007 4:05 PM | |
Posts: 17 Rating:
|
Hello Experts.... I am not sure where should I put this query, in Scada or PLC forum. anyways ... I am having a CPU 414-2 DP , aethernet CP 443 and WinCC communicating on ethernet with this CP. I want to show the Status of CPU RUN/STOP/System Fault in RT. I was trying to use evaluate " Tag Status" in Dynamic Diaglog. but, just imagine a case in which the CPU is in Stop mode , but the CP is in RUN mode. what will the Scada Display. Or, in short,do we have some SFC/SFB from where we can fetch the status of the CPU. I have seen FAQ http://support.automation.siemens.com/WW/view/en/19687561, "Displaying PLC status "STOP" on the Operator Panel" with follwing solutions
Do you have any Idea ?? My client is not ready to buy any AddOn Thank you... Regards Nitin |
9/20/2007 9:41 PM | |
Posts: 3149 Rating:
|
Hi do you use WinCC or WinCC flexible????? nemo |
9/21/2007 1:41 AM | |
Joined: 5/19/2006 Last visit: 8/21/2025 Posts: 550 Rating:
|
Have you seen this post? /tf/WW/en/Posts/5268 Dec |
Follow us on