(0)| 7/1/2014 12:22 PM | |
|
Posts: 3 Rating:
|
Unfortunately, the lincence is correctly installed, I have checked this..and still have the same problem. |
| 7/2/2014 9:33 AM | |
|
Posts: 3 Rating:
|
HelloK!ke Thanks for your reply. In fact, I have the WinCC RunTime Professional V11 installed.My project is a single PC Station linked to WinCC RT Professional V11 via Ethernet Modbus TCP/IP. I am trying to display the frequency from a Sentron PAC 3200 meter and see what will look like in runtime; The problem is every time I try to start the simulation , the RT won't start (it is grey) and this message error is displayed (attached file): "Software compilation started The project on the target device is closed Compiling aborted (errors: 0, warnings: 0)" Despite the number of errors and warnings recorded in the text of the last message, the number in the errors column for this message is 1. So I just want to start the RunTime simulation. Thank you for your help in advance.
|
| 7/3/2014 8:38 AM | |
|
Posts: 1299 Rating:
|
Hello, you have two different PCs, one with the engineering system wincc (tia portal) and one with WinCC Runtime Professional installed? And you are trying to download the configuration to the one with WinCC Runtime Professional? If I'm right, you can find the required settings here: http://support.automation.siemens.com/WW/view/en/88780011 K!ke |
Follow us on