(0)| 9/13/2012 6:48 AM | |
|
Posts: 8 Rating:
|
Dear all, I'm trying to repair a 55KW MM440 (6SE6440-2UD35-5FA1) with 1 blown up IGBT, P/N: BSM300GB120DLC_E3256, plus error code F0001. Attached is the pictures of damages. I repalce the damaged IGBT with BSM300GB120DLC and checked the other 2 IGBTs, they are okay. The Motor is okay too. I repaired all damages on the board and powered up the inverter. Error code F0001 disappeared but as soon as I wanted to start the motor, the IGBT which was gone before (Connected to X100), exploded again. I noted that there is an IC, P/N: A1458, in IGBT's control circuit which sounds like Op-Amp to me. Can this IC cause such problem? I would like to appreciate your kind help will Best Regards Fariborz AttachmentDamages&Repairs.pdf (426 Downloads) |
| 10/30/2012 9:12 AM | |
|
Posts: 3 Rating:
|
The firing circuit was defective or some other IGBT was damaged. A1458 is not an analog IC
|
| 9/4/2014 4:50 PM | |
|
Posts: 4757 Rating:
|
New question published by AutoGen_446199is split to a separate thread with the subject MM440 75kW IGBT Problem. Best Regards Min_Moderator |
Follow us on