10/30/2007 12:26 AM | |
Posts: 6 Rating:
|
Hi! I have some problems with a migrated project. It used to run on v4 not to good so I migrated the project to WinCC 5.1 SP2 instead. It runs ok now but every now and then I get an error message in script diagnostics. If I repeat the same procedure in runtime as before I might not get an error message that time. I suspect the PC allocated's memory and after a month or so it must be restarted. Can someone give me a hint or an example on how to use the system functions of sysfree and sysalloc. I am pretty sure that is whats wrong but I have never used thoose functions before and the online help and FAQ does not give any examples. Zeb AttachmentDiagn_071025.zip (122 Downloads) |
10/31/2007 3:34 PM | |
Posts: 1776 Rating:
|
Hi, see the FAQ http://support.automation.siemens.com/WW/view/en/22727197 |
Follow us on