11/25/2014 9:07 AM | |
Joined: 9/13/2014 Last visit: 11/11/2024 Posts: 15 Rating:
|
HI I have a master drives 6se7015-0ep50 . that already configuration fixed setpoint mode and operation . i want change to terminal input analog and strip but i did not doing . you help me do . i change p368.01=1 p443.01=10 conection x101/9 and 10 to 0-10 volt dc x101/7 +24 x101/8 on/off p544.01=20 p561.01=18 but no run drive . i send you back up and you configuration start up with analog input and terminal . this is parameter for fixed setpoint .you give me parameter for analog input for speed mode Attachment15 daf MC Plus_tmp.zip (420 Downloads) |
11/26/2014 4:10 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello amircontrol, make factory reset. then follow the MC 1.6 compendium section 5.5.6.5 prompted start up or follow section 6.3 quick parameterization. The link to the compendiumMasterdrives MC1.6: http://support.automation.siemens.com/WW/view/en/23660019 While arriving on an existing plant with Masterdrives equipment and less experience with Masterdrives are given,the following sections of the compendium are providing a basic knowledge: (4.Function blocks and parameters) 5.5 Handling DriveMonitor 6.2Detailed parameterization 7.2.3Basic positioning 8.2 Profibus communication 9 Technology option F01with encoder- undpositioning sensing items sections9.6.1/2and 9.8.6/7 Function diagramsbasic functions (The best is printing them on paper)The link to theDriveMonitor tool: http://support.automation.siemens.com/WW/view/en/11769381 |
With best regards, |
|
Follow us on