1/20/2015 1:11 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello putta; On most drive systems I have used, analog inputs are control inputs, not power inputs. For example, analog inputs on a SiemensMM4 drive are on a 0-10 VDC range. You can use a potentiometer on that range to send a speed control signal to the drive. But the drive must recieve a fixed power input at its power requirement level (240 V, 480 V...). See this manual to understand analog control of a MM4 drive: Operating Instructions: MICROMASTER 420 0,12 kW - 11 kW Hope this helps, Daniel Chartier |
Follow us on