7/24/2015 1:55 AM | |
Joined: 9/27/2006 Last visit: 9/12/2025 Posts: 12407 Rating:
|
Hello Mn; You could start by reading the following document, and look at the available links, to have a general idea of the way memory is structured in a S7-300 CPU, and distinguish load and work memory areas: How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices? Your situation will depend on the exact part number (MLFB) of your CPU, depending on the age of the CPU it will use either a MC (RAM or EPROM) or a MMC as load memory. As a rule of thumb, the ration of load to work memory should be at minimum 1 to 1:5. That is a 64 kB memory card would be adequate for a CPU having 48 kB work memory; only very old S&-300s have that small a work memory. So please provide the MLFB of the CPU you want to use so we can help out. I would also be useful if you attach a screenshot of your memory settings, from the CPU properties, in HWConfig (runtime), and the type and size of the presently used memory card. Hope this helps, Daniel Chartier |
This contribution was helpful to
3 thankful Users |
Follow us on