7/24/2014 8:08 AM | |
Posts: 1368 Rating:
|
Hello, |
7/24/2014 5:00 PM | |
Posts: 87 Rating:
|
Hi If you can work with I-device, follow the attachment example for configuration. Or you can also use the LCom application,and work directly withTCP/IP. Hope this helps. Regards AttachmentPN_RT_B_SIMATIC_SIMOTION.zip (567 Downloads) |
7/31/2014 9:02 AM | |
Joined: 6/22/2006 Last visit: 3/7/2022 Posts: 156 Rating:
|
Hi, please have a look to this FAQ http://support.automation.siemens.com/WW/view/en/43165740 This is an easy way for communication via TCP/IP. With the ProjectGenerator SIMOTION easyProject you are able to integrate this function into your project in a very convinient way. Both you can find on the SCOUT Utilities&Applications DVD. Regrds Manfred |
1/4/2016 1:46 PM | |
Joined: 9/1/2005 Last visit: 8/22/2025 Posts: 4114 Rating:
|
New question published by KhanhLe is split to a separate thread with the subject connect profinet integrated port in simotionD with simatic manager. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on