(0)| 2/27/2008 8:17 PM | |
|
Posts: 163 Rating:
|
Hi there !
Could you please provide me with a tip to solve this ?
AttachmentLibrary_Issue.zip (288 Downloads) |
| 2/28/2008 10:04 PM | |
|
Posts: 2661 Rating:
|
This is strange and I have not seen this behavior so far. Please try the following and let's see if it solves the problem: 1. Verify that the library (for example PCS7 V7.0 Library) is properly installed and you can see it from File/Open. 2. Hide the library. 3. Open CFC editor. You should only see the PCS7 V7.0 Library Folder. 4. Close CFC editor. 5. Display the library (after browsing). 6. Open CFC editor and check if the block folder displays correctly. AttachmentDokument1.pdf (402 Downloads) |
Follow us on