(0)| 3/17/2016 10:01 AM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hello, Uhm, Step 7 5.5 SP4 is not released for Windows 8.1. The latest operating system you can use is Windows 7. In the following link is the compatibility tool from Siemens. In here, you can select the Siemens software and see what is compatible with one another. Attached is a print out I made for you. You can see which operating systems are released. So, I will not continue to work further on Windows 8.1....More problems could arise.. AttachmentStep7_5.5.pdf (326 Downloads) |
Last edited by: Oreca at: 3/17/2016 10:03:23 AMLast edited by: Oreca at: 3/17/2016 10:07:05 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on