4/24/2016 2:29 PM | |
Posts: 5 Rating:
|
Hi Thanks for your reply, do you have an example? Thanks Peter Wright |
4/24/2016 3:26 PM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35918 Rating:
|
In attachmentan example. In the B003, the value for the GAIN parameter is entered via the TDE. The B002 is then calculated as an analog amplifier the value. Configured is the GAIN in B003 2 decimal places. For 1.25 must be entered 125 in TDE. B002 multiplied as the value of B001 with 125. Therefore, after that again with 100 divided (B002, parameter V3). B001 is used to get the value from the analog input in the B002. Otherwise B001 does not have any function in the program and must not be changed. AttachmentOwn_analog_amplifier.zip (460 Downloads) |
4/24/2016 4:27 PM | |
Posts: 5 Rating:
|
Thanks I've done it a similar way. Thanks Peter Wright AttachmentAnalog Amp for TDE.zip (382 Downloads) |
Follow us on