4/28/2016 6:52 AM | |
Joined: 12/18/2014 Last visit: 9/4/2025 Posts: 35925 Rating:
|
Hello, here in attachment is a Data Log. It was created without an SD card. If the internal memory is full, the oldest entry is deleted to make free space for a new entry. Logging began at 6:33:00. A new Data Log is not created until the existing Data Log wired uploaded from the logo. Uploading is only possible on the Logo software. To read the STOP must be switched. Attachment192.168.178.31_2016-4-28 6-40-26.zip (217 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on