(1)| 7/12/2016 11:27 AM | |
|
Posts: 8 Rating:
|
Hi Team I have an user defined FB in Step 7. And I used it in multiple places. I would like to get the scanning sequence no of that FB. Can anyone help me. For Ex : FB100 is a Motor FB i used for 10 motors like M01,M02...M10. The Scanning sequence are M01,M02...M10 as per program call. Now i would like to get 1 in M01, 2 in M02 as scanning sequence number. Please let me know how to do program to get this value in FB? Thanks and Regards Ramesh D ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/12/2016 12:54:51 PMNew subject after splitting |
|
| 7/13/2016 10:18 AM | |
|
Posts: 5225 Rating:
|
Hi. I have read again the original post where yours were linked from. The answer is actually written there. If you are using LAD / FBD / STL language, then the STL instructions are..
I you are using SCL then you need something else. You need to take one on the parameters of the FB and "create" an ANY variable from it. Review again what is written by
GrzegorzG
in the original post - w |
Follow us on