8/24/2016 4:44 PM | |
Joined: 3/20/2012 Last visit: 9/5/2025 Posts: 120 Rating:
|
Hi evrybody, I'm looking for the wiring diagram for 64Do (6ES7 322-1BP00-0AA0). I've found the manual with the wiring diagram, but it seems to be false! https://support.industry.siemens.com/cs/fr/fr/view/8859629 At page 134 you can see that the first two wires are not wired the same way on the second group! The real question is: I have to make myself the cables from the 64DO card and i'm not sure that the numbers from the table in page 136 are the same on connectors X1 and X2. Any idea? Thanks. |
Follow us on