10/22/2008 4:57 PM | |
Posts: 34 Rating:
|
Hi all, We're planning a project that uses up 20 (maybe more in the future) Panels - TP177 4" Color PN/DP. We'd like to connect them all to 1 controller (S7-31x or WinAC), using profinet for communication with the PLC. Looking at the PLC specs, there are several types of communications functionsthat all have a different number of max. connections. eg. CPU 315-2 PN/DP -Open IE-Max. Connections: 8 - Number of usable OP Connection: 15 - Profinet CBA: NA for TP177 - 2nd Interface as Profinet IO Controller - Max. Connectable IO Devices: 128 Is it possible to connect up to 128 Panels onto this CPU or is it restricted to 8 or 15 Panels? willan Lean CP card give me the possibility to extend this amount of connectable Panels. Tx in advance, HG AttachmentCPU 315-2 PN_DP.pdf (471 Downloads) |
Follow us on