12/7/2016 11:41 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating:
|
Hi Bora, I hope you have set address in hardware configuration. This is default setting.You must configure the communication connections in the project engineering. Also compile and download NETPRO. Otherwise prepare PLC program for using IP_config and send/receive blocks and download. You can also refer manual: S7-CPs for Industrial Ethernet Manual - Configuring and Commissioning. Also you should publish this topic Communication / Networks conference. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on