1/22/2017 8:46 PM | |
Posts: 4 Rating:
|
I have a 6es7 315 2ag10 firmware v2.0 PLC and tried to use it in TIA portal V12. As I tried to go online, it shows error. Difference in firmware version Online V2.6 <-> V2.0 offline. Also I have 8MB MMC card for load memory. If I upgraded the latest firmware does it solve the problem? I want to use the old PLC with a MP277 10" HMI with profibus. Please help... ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/23/2017 3:24:47 PMNew subject after splitting |
|
1/22/2017 8:57 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, check below if your CPU is supported in TIA: http://support.automation.siemens.com/WW/view/en/60162195 https://support.industry.siemens.com/tf/WW/en/posts/firmware-update/98760?page=0&pageSize=10 |
Last edited by: Ste39 at: 1/22/2017 9:13:54 PM |
|
Follow us on