3/6/2017 9:30 AM | |
Joined: 10/18/2012 Last visit: 9/12/2025 Posts: 225 Rating:
|
Hello NPSK, I remember some issue with WinCC SQL database instance some time ago. The software was unable to install because of an existing WinCC instance. If you want to install the whole operating system new, then you can use a normal windows setup CD or DVD with the following limitations: Alternatively you can order the original Setup-DVD from Siemens Technical Support. You need the exact article number of your IPC477D. It is something like 6ES7... Siemens Technical Support can be found here: regards, |
Follow us on