7/30/2017 2:08 PM | |
Posts: 13 Rating:
|
Hi all 1: ---Deleted Link, look attachment--- If you open this printscreen you see an analog input A3 (pt100), B134 is the analog amplifier to convert to temperature. next i have B213 that simply sets an offset because there is a little bit of difference between real temperature and logo temperature. Is there something that misinterpreted? Here you see a simple test. B124 is a mathematic instruction. On the left you see the situation in simulation, there is a value P1 is 348 that i can put there from message text. you also see that the parameter Aq is 348 so i can use this value elsewhere. Now when i download that program and test online, you see the situation on the right side. The P1 value is still 348 but the Aq parameter is set to 0. Why is that? Why is there a difference between simulating and online test? Robby Attachmentpictures.zip (156 Downloads) |
Last edited by: Jen_Moderator at: 8/1/2017 8:38:16 AMAdded pictures as an attachment. |
|
7/30/2017 3:40 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
These are only differences in the displaying between simulation and online watching. The values in the expanded list field for the reference function have only real validity in the simulation. See attached video. AttachmentOnline.wmv (165 Downloads) |
7/31/2017 4:55 PM | |
Posts: 13 Rating:
|
Ok, this makes it very confusing. Thanks for the answer. |
This contribution was helpful to
1 thankful Users |
Follow us on