(0)| 8/25/2017 1:00 PM | |
|
Posts: 17 Rating:
|
I have 3 iot2040 applications that all need a kernel module that is not in the Siemens provided flash image. Consequently I have to run Yocto because the Linux headers are missing. I must admit that I am very disappointed with the support from Siemens on this product, because there is no supported way of using the Yocto industry standard to get customers out of this type of problems. Why not release a Yocto-setup article that is checked and working? Regards An owner of 3 iot2040 boxes waiting for its Linux. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 8/30/2017 10:10:34 AMNew subject after splitting |
|
| 8/26/2017 7:26 PM | |
|
Joined: 4/28/2015 Last visit: 1/7/2026 Posts: 578 Rating:
|
Yocto is a tricky beast, indeed. That's why our expert group at Siemens started the kas project (https://github.com/siemens/kas) to make (re-)building images much easier than with most approaches you find out there in the wild. It's still a young project that may miss a few remaining corner cases. So please follow up in the other thread (https://support.industry.siemens.com/tf/ww/en/posts/which-way-is-successfully-to-create-an-image/176288/?page=0&pageSize=10#post702435) to help us sorting them out, for the IOT2000 and beyond. Thanks! |
Follow us on