9/6/2017 8:34 PM | |
Posts: 56 Rating:
|
Hello friends, I'm trying to create a program for controlling the pellet boiler. It should behave according to the attached graph. After a certain amount of time, it must change the AQ value. The AQ value in the graph is just an example, the times are tested. Changing the AQ can be jumping or "interpolation". I just do not know if Logo! he can, and if so, I have not come to it yet. Excuse my English (I'm consulting with the translator) and if you have a suggestion, I'm here with him. Thanks Ladislav Ahoj kamarádi, snažím se vytvořit program pro ovládání kotle na pelety. Měl by se chovat podle připojeného grafu. Po určitém čase musí změnit hodnotu AQ. Hodnota AQ v grafu je jen příklad,časy jsou vyzkoušeny.Změna hodnoty AQ může být skoková nebo "interpolací". Jen nevím zda to Logo umí, a pokud ano zatím jsem na to nepřišel. Omluvte mou angličtinu (radím se s překladačem) a pokud máte nějaký návrh, sem s ním. Díky
Attachmentgraf.pdf (183 Downloads) |
9/6/2017 9:27 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
In attachment a possible solution. AttachmentTime-controlled_analog_output_0BA8.Standard.zip (187 Downloads) |
This contribution was helpful to
1 thankful Users |
9/8/2017 9:06 PM | |
Posts: 56 Rating:
|
Hi ixo, here is a new chart of how the program should behave. Unfortunately, I'm not even able to implement this change. Will you help one more time? Thank you very much Lada
AttachmentGraf 2.pdf (142 Downloads) |
9/8/2017 9:36 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35961 Rating:
|
Here's the second version. But I don't make for you every day an extension for the circuit .... AttachmentTime-controlled_analog_output_0BA8.Standard_V2.zip (132 Downloads) |
9/8/2017 9:57 PM | |
Posts: 56 Rating:
|
if I knew English and had time, "I do not like to stay" |
Follow us on