10/23/2017 1:04 PM | |
Joined: 1/30/2006 Last visit: 5/15/2025 Posts: 310 Rating:
|
Hi Rizlan Take a Look at the Analog MUX. I think that's the answer for your problem |
BR. Sven |
|
10/23/2017 1:41 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35962 Rating:
|
Hello Rizlan, in attachment is a simple example. With the analog MUX, you are able to output up to 5 values. No input active = 0. The given values are only in this example, you can enter them in the block properties according to your wishes. Since the analog output outputs 10.00 V at 1000 units, 5V = 500 units AttachmentAnalog-MUX_0BA8.Standard.zip (186 Downloads) |
This contribution was helpful to
1 thankful Users |
10/24/2017 6:38 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35962 Rating:
|
In attachment a possible solution. AttachmentAnalog-MUX_V2_0BA8.Standard.zip (174 Downloads) |
Follow us on