10/24/2017 8:36 PM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello moji; Here are some documents that should enlighten you, to start your projet evaluation: In order to make a complete flowmeter, the SITRANS FCS200 sensor must be combined with the following MASS transmitter:SIFLOW FC070: For direct integration into SIMATIC based systems, or used as stand alone with non SIMATIC systems. The FC070 is designed for the S7-300 backplane, but can also be used with a remote Profibus-DP or Profinet link, as part of an Et 200M installation (with an IM 153-2 or IM 153-4). Note this important information : 6.2 Installation of S7 Hardware support package The SIFLOW FC070 function module is not located in the S7 module catalog, but is subsequently installed using a hardware update (Hardware Support Package "s7h2008x.hsp"). This hardware update contains the user GUI for HW-Config and online help. This information is valid for Step 7 v5.x, here is a solution for TIA Portal: Support Packages for the hardware catalog in the TIA Portal (HSP) SIFLOW FC070 software for SIMATIC TIA portal - ID: 81527994 Hope this helps, Daniel Chartier |
This contribution was helpful to
2 thankful Users |
10/25/2017 11:35 AM | |
Posts: 6 Rating:
|
hi. thanks for your answar. but there isnt information about my question in this documents. i want use fcs200 with cpu 1212c but i cant find aout it. |
Follow us on