1/8/2016 11:12 AM | |
Joined: 10/23/2015 Last visit: 8/15/2025 Posts: 168 Rating:
|
hi, i have a problem with the same product (PAC3200), it is not "visible" on the Network profinet. Please help Thanks ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 1/10/2016 10:47:11 AMNew subject after splitting |
|
8/23/2016 3:42 PM | |
Posts: 3 Rating:
|
Thank you very much. Now, it is working properly after I set the Profinet name as you described. |
4/30/2018 2:53 PM | |
Joined: 8/15/2008 Last visit: 12/15/2023 Posts: 32 Rating:
|
Hello, my CPU is 315-2PN/DP and programming media is STEP7 v5.5. I also don't see configured PAC3200 (with ethernet module switch) on network, in spite of the fact, that I can ping it and see on accessible nodes. Attached are screenshots. Could you please point out what is wrong with configuration ? Regards, Samir AttachmentPAC3200.pdf (930 Downloads) |
Last edited by: samir_a at: 4/30/2018 3:04:24 PM |
|
5/1/2018 8:45 AM | |
Joined: 8/15/2008 Last visit: 12/15/2023 Posts: 32 Rating:
|
I've found the solution. First, I've replace old GSDML file with new one (link to download https://support.industry.siemens.com/cs/ww/de/view/59840946 / "GSDML_for_PAC3200_PAC4200_V2_3.zip" file). After installing new GSDML file, I deleted the old PAC device in my hw config and created a new one. Then I go online in Simatic Manager -> Display accesible nodes and by selecting required ethernet node of PAC3200, go to PLC -> Diagnostic/Setting -> Module information. Here in popup window of "Edit Ethernet Node" I assigned device name for configured PAC3200. After these procedures I succeeded to see PAC3200 in hardware config. Hope it will help others, thank you. |
Last edited by: samir_a at: 5/1/2018 8:50:14 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on