9/11/2018 5:07 PM | |
Posts: 1 Rating:
|
Hi! Im new in this area When i start node-red on putty appear this error message "No response from PLC, restarting communication" and "Error connecting to PLC: Error - TCP connected, ISO didn't ", i don't know where is the problem! Thanks ! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/12/2018 6:57:23 AMNew subject after splitting |
|
12/10/2018 8:00 PM | |
Posts: 2 Rating:
|
Good day.. Im experiencing same issue as stated.. FYi Im attaching the NR flow and other images that can help Version of the PLC 1200 is V3 and the node red is 0.19.. Note that the PLC program was created in TIA V12 and im using TIA V13 so please keep in mind that if for instance u ask me to change something. All these files are zipped In advance, thanks a lot for your help AttachmentNR_S7_Issue.zip (222 Downloads) |
Follow us on