1/27/2019 1:24 PM | |
Posts: 6 Rating:
|
Bonjour, j'ai un CPU 414-5hm06-0ab0 et deux indicateurs qui restent orange à droite. ------------------------------------------------------------------------------------------ |
Last edited by: zouz at: 1/27/2019 1:28:25 PMLast edited by: zouz at: 1/27/2019 1:29:10 PMLast edited by: Jen_Moderator at: 1/28/2019 7:15:03 AMNew subject after splitting |
|
1/27/2019 4:03 PM | |
Joined: 9/27/2006 Last visit: 9/17/2025 Posts: 12411 Rating:
|
Translation from the French text;
Bonjour zouz; On vous a déjà demandé d'utiliser l'anglais sur ce forum, prt respect pour les membres qui ne parlent pas français. Si l'anglais est exigeant, nous pouvons vous suggérer des traducteurs électroniques tel Google Translate. Je ne suis qu'un simple participant au forum de Siemens, comme vous, qui essaie de vous rendre la vie plus facile. De plus, il serait beaucoup plus simple eyt plus efficace d'ouvrir un seul fil pour toutes vos questions concernant votre CPU, plutôt que de vous disperser à travers des fils existants. Pour ce faire, ouvrez la conférence S7-400/S7-400H dans la colonne de gauche, vous verrez un bouton rouge marqué "New Topic". Merci de votre attention. Hello zouz; You have already been asked to use English on this forum, out of respect for members who do not speak French. If English is demanding, we can suggest electronic translators such as Google Translate. I'm just a participant in the Siemens forum, like you, trying to make your life easier. In addition, it would be much simpler and more efficient to open a single thread for all your questions about your CPU, rather than scattering through existing threads. To do this, open the S7-400 / S7-400H conference in the left column, you will see a red button marked "New Topic". Thank you for your attention. One more recommendation: if you are working with a S7-400H CPU, you should keep the S7-400H manual close-by, it is there you will find installation and operation details that can ease your mind. Look at the attachment below showing that thes active LEDs are sinply indicating that the CPU is operation normally. Note that most of the Siemens manuals can be downloaded in other languages than English. If you click on the Language link for this manual, you will see a French version available to you. https://support.industry.siemens.com/cs/ww/en/view/82478488 Hope this helps, |
Last edited by: dchartier at: 1/27/2019 4:05:44 PMLast edited by: dchartier at: 1/27/2019 5:39:25 PM |
|
1/27/2019 5:55 PM | |
Posts: 6 Rating:
|
thank you very much, your answers are always welcome. and I will try to write in English of course. |
Follow us on