(0)| 2/15/2019 6:18 AM | |
|
Posts: 10 Rating:
|
Good evening, experts. I have a PLC s7-200 CPU 224, a EM232 module, photoelectric sensors, electropneumatic positioners. Attached a picture of the diagram in staircase I describe roughly what I want to do. What I seek to realize is that automatically when the input I0.0 is in high state, send activate an engine, and in turn send 8 ma through one of the outputs of the module em232 to send activate a positioner Electroneumatico and when the sensor I0.1 is It is in high condition that it sends 4 ma and that it stops the motor, until the sensor I0.0 is again in high state. I've been reading about scaling |
Last edited by: angels at: 2/15/2019 6:20:31 AMLast edited by: Jen_Moderator at: 2/15/2019 11:22:05 AMOptimized link. |
|
Follow us on