4/2/2019 10:37 PM | |
Posts: 2 Rating:
|
I have a Miltronics Multiranger 100, SN:051904111XC that has connect to XPS-10. All worked good in this equipment during long time. The system battery had discharged. I change the battery. Now, after start, the Multiranger printing the message 'tb4: open' and not changhe the level on monitor. I have handhield programmer. I set 1954 in P069 and 1954 in P000, but i can not change P001, that has value 67. I set 00 and 0 to P999, but all parameters don't change value. The LED D52 on mother board is blinking. I placed sensor XPS on other input on mother board, but nothing changes. Black wire of sensor I placed to "+" on mother board, white to "-", shielding wire had been conected to ground. Why I can not change P001 and other parameters in Multiranger? ------------------------------------------------------------------------------------------ AttachmentMultiranger.pdf (312 Downloads) |
Last edited by: Jen_Moderator at: 4/3/2019 11:36:29 AMNew subject after splitting |
|
Follow us on