8/1/2019 8:58 PM | |
Joined: 9/27/2006 Last visit: 9/15/2025 Posts: 12408 Rating:
|
Hello Zay: Start by have a look at this extract from the Masterdrive Compendium: http://samsebeplc.ru/Doc/Siemens/SIMOVERT/vc33_kompend_kap082_e.pdf This FAQ should also be helpful, even though is is dedicated to Masterdrive VC drives; there is also a sample function showing how to start and stop the drive.: Connection of Masterdrives to Profibus-DP. https://support.industry.siemens.com/cs/ww/en/view/20386822 Hope this helps, Daniel Chartier Edit: Soprry, I just realized I pointed to the manual for Masterdrives VC, instead of the inteded MC. Here ios a link to the MC Compendium (system manual): study chapter 8.2 Attachmentvc33_kompend_kap082_e.pdf (386 Downloads) |
Last edited by: Jen_Moderator at: 08/02/2019 10:57:19Added pdf file as an attachment. Last edited by: dchartier at: 08/02/2019 19:51:31 |
|
This contribution was helpful to
1 thankful Users |
Follow us on