5/18/2020 3:55 PM | |
Posts: 1 Rating:
|
Hello, Did you find something that help you ? I have the same issue, I don't find any RoHS certifcate or the REACH for the CPU 1511-1-PN (6ES7511-1AK00-0AB0) ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/19/2020 08:35:53New subject after splitting |
|
5/18/2020 4:11 PM | |
Joined: 9/27/2006 Last visit: 9/7/2025 Posts: 12401 Rating:
|
Hello blig: See if the following document can answer your question on REACH and RoHS for Siemens products: Information about product-related environmental protection https://support.industry.siemens.com/cs/ww/en/view/39200038 - Are the products in compliance with the REACH regulations, are all the substances in the delivered products registered or are there substances that are on the REACH Candidates List? Siemens DI, SI CP and SI LP fulfill the obligations defined in the REACH Regulation. Siemens DI, SI CP and SI LP have pre-registered all substances subject to registration that are manufactured or imported by Siemens in due time and will register them at the specified times, if necessary.. - Do the products meet the valid restrictions for the use of hazardous substances as per Directive 2011/65/EU (RoHS)? We confirm that the products supplied by Siemens DI, SI CP and SI LP that fall within the scope of the RoHS Directive 2011/65/EU meet the requirements of the RoHS Directive. The conformity of a product with the RoHS Directive and the national laws implementing the RoHS Directive is confirmed by the EU Declaration of Conformity. Detailed information on compliance with substance restrictions in accordance with Art. 4 of the RoHS Directive can be found product specific in the Siemens Industry Mall (online ordering system). Additional requirements must be specified in separate agreements. Hope this helps, Daniel Chartier |
Follow us on