(0)| 5/28/2020 12:20 PM | |
|
Joined: 8/3/2009 Last visit: 1/23/2026 Posts: 16661 Rating:
|
Hello check in the Step7 Project path if there is a Folder "HMIES" if yes then look if there are the HMI Files *.hmi and *.ldf If yes, try to open the HMI File with winCC flexible. If the files are there but you do not see the Panel in your Simatic Manager project then it could be that the integratino SW is not installed -> you can install it from Flexible DVD -> or the Intregration of the Flexible Project in the SImatic Manager Project is damaged then LINK Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on