(0)| 6/9/2020 11:32 PM | |
|
Joined: 9/27/2006 Last visit: 1/21/2026 Posts: 12481 Rating:
|
Hello TeoTheNtal; In FB 41 CONT_C the only occurrence of the word "HOLD" is the INT_HOLD parameter, which controls the application of the Integral gain. See the following diagram and tell us if that is the parameter you are inquiring about: PID Cont_C FB 41 diagram https://support.industry.siemens.com/cs/ww/en/view/589983 CONT_C is designed so that you can use it as a simple P controller, a PI controller, a PD controller (not very stable, not easy to tune) and a full PID controller. You do that by enabling or disabling the integral or derivative calculations that the function is doing, before launching the controller. The INT_HOLD parameter stops the integral action in the controller, which tends to smooth pout the variance of the error over time. If your loop was tuned as a PID or even a PI controller, then stopping the integral action would make the control purely reliant on the error (PV_SP) in the system, multiplied by the proportional gain factor of the loop parameters.In other words, it would tend to make the loop response less stable, more unstable as the error grows. In certain processes, we have blocked the integral portion of the loop to stop the integral action of a PI or PID controller, in order to "give a boost" to the final action element, when its response is sluggish. But generally this should be a short-term solution, in the long term. The screenshot below is taken from the System and Standard functions manual , section 28.1 (for the S7-300 and S7-400 CPUs). You can check with the Step 7 online help if anything has been changed for its operation under Step 7 Professional. https://support.industry.siemens.com/cs/ww/en/view/109751826 Hope this helps, |
Last edited by: dchartier at: 06/09/2020 23:36:00Last edited by: dchartier at: 06/10/2020 00:00:59 |
|
This contribution was helpful to
|
|
Follow us on