10/11/2020 4:57 PM | |
Posts: 1 Rating:
|
Dear engineers, I as currently working on one project where I am planning to use Siwarex 231. It is linear weighing system for berries. I am wandering is Siwarex able to do the task which I am going to describe below or I need to have additional PLC. My task is: I am planning to fill berries in 5 kg boxes and dosing unit will be electro magnet shaker. Weighing unit will measure the weigh in boxes. When process starts, shaker will start to move in desired speed and it is rough dosing. When the weigh in boxes reaches one value e.g. 80% of measure (4 kg) then Siwarex should send the analog signal to electro magnet shaker to decelerate the speed until it reaches desired weight (5kg). This phase is fine dosing. After that process stops, and then starts over. So, is it possible with Siwarex 231 or I need PLC additional modul? Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2020 10:56:17New subject after splitting |
|
10/14/2020 8:43 AM | |
Joined: 1/4/2007 Last visit: 8/26/2025 Posts: 1190 Rating:
|
Hello bozaue, The Siwarex WP231 can NOT handle such an application. Here, you have to use an additional PLC OR you use the Siwarex WP251. The Siwarex WP251 can handle dosing applications. When you have no PLC, then you have to set the parameters in the WP231/WP251 module with the Siwatool-software. The order-number for the Siwatool-software is: 7MH4900-1AK01 Best regards Siwarexi AttachmentFlyer_SIWAREX WP251_EN.pdf (348 Downloads) |
Follow us on