(1)| 11/18/2020 4:02 PM | |
|
Posts: 152 Rating:
|
Hi guys, On Unified panels with Image update 1 and Image update 2 it is only possible to use Sm@rtClient on port X2. With Image update 3 it is now possible to use Sm@rtClient on both X1 and X2 port. Here is the link for downloading Image update 3 for Unified panels: https://support.industry.siemens.com/cs/ww/en/view/109746530 |
Last edited by: Jen_Moderator at: 11/19/2020 09:22:52Optimized link. |
|
| 11/20/2020 5:07 AM | |
|
Posts: 54 Rating:
|
Yes I meant X1 and X2 the reason I mixed it up is because when I download to the panel it says slot 5 and 6 :)
How can I see which update I´m using? I tried installing update 3 and downloading to the display without luck. P.S.If it´s a firmware issue I was not able to choose any other firmware after installing update 3. |
Follow us on