2/3/2021 1:09 PM | |
Joined: 6/30/2014 Last visit: 8/4/2025 Posts: 475 Rating:
|
Dear Nek4926, can you add some further information about this point? Maybe you can see with the DebugView or even the ProcessMonitor from Microsoft what is wrong, in the logs? Here you see a good FAQ. In case you are sure that this is a kind of bug in COMOS itself and it can be rebuild, you should open a ticket. All the very best, SuperPippo |
Follow us on