2/4/2009 8:31 PM | |
Posts: 11 Rating:
|
Hi everybody I have an FC (in this case FC54) and it works well when I call it from FC47. In file1.jpg you can see a segment of FC47 calling FC54. The problem is this: in the same FC47 I need to add a segment calling FC54, so I add the segment and when I compile it there is a trouble; something about a conflict between the input types. You can see the segment added in file2.jpg and the error message in file3.jpg (it's in spanish, sorry). So, I don't understand why this error??? ... if I am only calling an existing FC ... Please, help me with this. Best regards Attachmentfiles.zip (330 Downloads) |
2/4/2009 10:41 PM | |
Posts: 2661 Rating:
|
Hi Metal_Kain, The problem is not with FC54, but a "non-existing" symbol D_UB11 in the symbol table. Regards |
2/5/2009 6:04 PM | |
Posts: 11 Rating:
|
hi Phantom75 that's not the problem ... 'cause I'm using D_UB11 in another segment, it's defined in the table. any other idea???? |
2/5/2009 11:21 PM | |
Joined: 10/7/2005 Last visit: 9/4/2025 Posts: 3049 Rating:
|
Hello Metal_Kain try this: 1.) Remove the invalid "D_UB11" N/O contact in NW 100 and save FC 47 2.) Change to FBD 3.) Add "D_UB11" via aFBD AND gate to the EN input of FC54 4.) If this does not give you an error and you can save the block youwill (should) also be able to change back to LAD now (and came blame the Step7 LAD Editor for the problem, I had this issue a few times too myself and trust Siemens will fix it soon). I hope this helps Cheers Fritz |
Cheers |
|
2/6/2009 2:17 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Dear Metal_Kain, What version of Step 7 are you using? Best regards, Wizard |
2/6/2009 2:42 PM | |
Posts: 11 Rating:
|
Hi Wizard I'm using: V5.4+SP2, release:V5.4.2.0 Best regards |
2/6/2009 3:08 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Dear Metal_Kain, Please download Service pack 4 for Step 7 v5.4: http://support.automation.siemens.com/WW/view/en/29753195 It will solve your problem. Best regards, Wizard |
Last edited by: Wizard at: 2/6/2009 3:11 PM |
|
This contribution was helpful to
1 thankful Users |
2/6/2009 8:05 PM | |
Posts: 11 Rating:
|
Hi Wizard I'm downloading ... then I'll try Thanks for your help. |
Follow us on