2/15/2021 12:34 PM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
Hi engineeeer, there is also an FAQ for that, maybe this helps. What is the effect of the STEP 7 function "Copy RAM to ROM"?"In the case of CPU modules that have a built-in EPROMyou can use the "Copy RAM to ROM..." function to copy the content of the internal RAM load memory to the built-in EPROM load memory so as not to lose data in the case of power failure without battery or overall reset." regards sancruz
|
Feedback appreciated, please rate |
|
This contribution was helpful to
3 thankful Users |
2/15/2021 3:58 PM | |
Joined: 4/24/2006 Last visit: 7/31/2025 Posts: 9027 Rating:
|
Hello engineeeer, Why would you delete blocks from MMC? Just perform the command: "Copy Ram to Rom". What did you change? I guess it were some actual values in DB? When you download your Program it is downloaded to MMC (Always remanent) The command "Copy Ram to Rom", only overwrite the actual values from DB to initial values. Best regards, Wizard |
Last edited by: Wizard at: 02/15/2021 16:02:22 |
|
This contribution was helpful to
1 thankful Users |
2/18/2021 10:59 AM | |
Joined: 1/4/2019 Last visit: 6/1/2024 Posts: 60 Rating:
|
Thank you wizard and thank you all , I didn't delete the MMC just to show you the procedures . I make the changes and make "copy RAM to ROM" as you said and its successfully succeeded . Thank you all for your precious help. |
This contribution was helpful to
1 thankful Users |
Follow us on