3/2/2021 6:57 PM | |
Joined: 2/17/2021 Last visit: 4/12/2023 Posts: 7 Rating:
|
Gibernaus, Thanks for your input. I can see how MD36912 might make things better. I tried two things and I'll detail them below. First thing I tried:
The result was no alarms at boot time but when I tried to move the axis it immediately alarmed with a position mismatch. It seems the resolution of encoder 1 doesn't match what the SPL was expecting. In the SI, SPL display the position was 0.100mm on one side and about 0.900mm on the other side. Second thing I tried:
The result here was a ton of alarms at boot time. All the alarms had to do with the other axis (NOT the one I'm modifying) With the alarms I was unable to bring the machine up to try moving it. In this case the SI, SPL display for drive #5 (Z3) was blank as you suggested it would be. I'll include some pictures of this condition. I really appreciate all your time and help Justin Attachment840d_errors.zip (144 Downloads) |
Last edited by: seneca-machine at: 03/02/2021 19:41:16 |
|
Follow us on