2/3/2021 9:20 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
I can tell only the same: You don't understood ... |
2/3/2021 9:25 AM | |
Joined: 12/18/2014 Last visit: 9/16/2025 Posts: 35964 Rating:
|
You cannot suggest a solution to the problem because there is no solution. The "LSC & LWE Access" function in the Access Control menu is only valid for LOGO!8.3. This is why it is grayed out in LOGO!8.2 and all older 0BA8 LOGO!s and has no function. The check mark cannot be removed for the same reason. In the attachment a screen video showing the effect by a LOGO!8.3, with password and without password.
AttachmentLSC & LWE Access.zip (551 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on