4/17/2007 9:01 AM | |
Posts: 65 Rating:
|
Dear Ikkezelf, Where are the diagnose folders located? What type of file should i look out for? Regards Schreyer |
4/17/2007 11:08 AM | |
Posts: 1084 Rating:
|
Hi, The folder will always be there. Not only the errors are being logged, also success. We'll see them appear. regards, Ikkezelf |
5/3/2007 4:28 AM | |
Posts: 65 Rating:
|
Dear Ikkezelf and all, I have the diagnose folder zip for server1, but i do not know what to look out for. Can somebody help me out here? Regards Schreyer AttachmentServer 1 diagnose.zip (370 Downloads) |
5/3/2007 4:29 AM | |
Posts: 65 Rating:
|
Dear all, Attached is for server 2. Thanks once again for the help. Regards Schreyer AttachmentServer 2 diagnose.zip (364 Downloads) |
5/3/2007 9:42 AM | |
Posts: 1084 Rating:
|
Thanks, several references I see, but none of them rings a bell for me. I will notify Danielle and Nemo to have a look at this. with regards, Ikkezelf |
5/3/2007 1:41 PM | |
Posts: 1275 Rating:
|
Hi, I'm taking a look at the diagnose folders now, and there are a couple of things I noticed, and some will probably have nothing to do with the communication error, but you should still clear these out: Server 1: 65535,30.04.2007,14:41:03:913,1001003,8,,SERVER1,PDLRuntimeSystem,,,0,0,0,Picture not found (notvalid.PDL),,, Both servers 1 and 2: 255,20.04.2007,20:34:33:707,0,4,,SERVER1,ArchiveManager,Failed to switch archive(Type:2):(null) ! Check this post out, and also this one. One of them says that if you're under v5 this isn't a real problem, it's just a tracing utility from WinCC. 255,30.04.2007,14:15:36:556,1007001,4,,SERVER1,SCRIPT,ExecuteError in Action @ee9 255,30.04.2007,14:16:36:450,1007006,4,,SERVER1,SCRIPT,Variable MM6_1001E_.OPSHRS timeout 2007-02-24 11:13:00,432 ERROR Connectionerror "Main": OpenRef=0019 Confirmation timeout! 2007-02-24 11:13:00,432 ERROR StartDisconnect "Main": OpenRef=0019 2007-02-24 11:13:00,432 ERROR StartDisconnect "Main": OpenRef=001A 2007-04-03 11:02:40,677 ERROR Connectionerror "Gpp5/6utility": OpenRef=000F Confirmation timeout! 2007-04-03 11:02:40,677 ERROR StartDisconnect "Gpp5/6utility": OpenRef=000F 2007-04-03 11:02:40,677 ERROR StartDisconnect "Gpp5/6utility": OpenRef=0010 2007-04-03 12:14:23,470 ERROR Connectionerror "Gpp5/6utility": OpenRef=0073 AWAIT_CLOSE iNAResp=16! 2007-04-03 12:14:23,470 ERROR StartDisconnect "Gpp5/6utility": OpenRef=0073 2007-04-05 10:49:58,730 ERROR Connectionerror "GPP5": OpenRef=0017 Confirmation timeout! 2007-04-05 10:49:58,730 ERROR StartDisconnect "GPP5": OpenRef=0017 2007-04-05 10:49:58,730 ERROR StartDisconnect "GPP5": OpenRef=0018 2007-04-05 10:52:59,747 ERROR Connectionerror "GPP5": OpenRef=0019 AWAIT_CLOSE iNAResp=16! 2007-04-05 10:52:59,747 ERROR StartDisconnect "GPP5": OpenRef=0019 2007-04-05 11:15:55,400 ERROR Channel PES/API error "No Request Object available for confirmation." About these last ones check this post. I'm still looking for something else. If I find anything I'll post. Best regards, Danielle |
Follow us on