10/6/2009 5:20 PM | |
Posts: 2661 Rating:
|
This is exactly the message I get when I remove the sharing on the server project folderand try to change screens on the client. Was your system working before or it never worked properly? Seems likeyour problem is network related. Couple of FAQ's worth checking: How do you use the SIMATIC shell to configure the terminal bus of a WinCC station? How can you clear the error message "Download (310:88)"? Regards |
10/9/2009 9:27 PM | |
Posts: 2661 Rating:
|
First step is to identify what settings were changed to configure the OPC client? IMO a WinCC client should be dedicated as an OPC server so that settings of only this machine need be changed. Is it possible to go back to original (pre-OPC client) configuration? Also please verify the DCOM settings (in the SIMATIC-NET manual)fromthe following link: Which settings should you check if OS downloading fails with PCS 7 or the OS project cannot be activated? Regards |
Follow us on