11/1/2021 7:54 PM | |
Joined: 4/28/2015 Last visit: 4/25/2025 Posts: 17 Rating:
|
LSC updated to LSC V8.2 SP1. The issue still here. What firmware files should i use , the one found at LSC V8.2 SP1 or this one FW_Update_Fix_TALOS-2020.zip (1,2 MB) ? |
11/1/2021 8:08 PM | |
Joined: 12/18/2014 Last visit: 9/12/2025 Posts: 35955 Rating:
|
The last one that I linked, it's the current version. |
11/3/2021 5:10 PM | |
Joined: 4/28/2015 Last visit: 4/25/2025 Posts: 17 Rating:
|
" you do not write .... " You could also have asked Let´s confirm once more the information. The firmware is from this Link right ? Product information on the firmware update for LOGO! 8 for security Vulnerability CVE-2020-7593 LOGO has V1.81.01 firmware. I am using Windows 10 but i have already tested with a virtual machine with W7 and the Data table problem is there. For firmware update i have used the files found at installation of LSC V8.2 SP1 , perhaps is this the problem of not being able to update the firmware ? Later i will try to update the firmware using the files of this Link. Product information on the firmware update for LOGO! 8 for security Vulnerability CVE-2020-7593 Regards, MD |
Follow us on