3/1/2013 8:49 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
hello, Lot of questions
Start with manual, there you will find how to connect the onboard i/o. You don't have to configure the onboard i/o, that's already done because it's a compact CPU. You can however change the configuration, but better leave it as it is. Analog inputs are read as PIW xxx , outputs are addressed PQW xxx, you will find the xxx in the hardware config. Channels are the analog inputs/outputs, channel 1 is your 1st analog input. Yes, you can use i.e. a 9 V battery if analog input is 0-10V (default setting) To process the analog value you may need to scale the analog input signal. I have attached some screenshots to show some things. If any more questions, ask. Regards, Marcjan Attachmentanalog_forum.pdf (930 Downloads) |
Last edited by: Marcjan at: 3/1/2013 8:55 AMLast edited by: Marcjan at: 3/1/2013 8:50 AMProblem solved? |
|
6/27/2014 6:41 PM | |
Joined: 3/25/2013 Last visit: 4/7/2025 Posts: 176 Rating:
|
New question split intoconfigure pt100 on s7300. With best regards, Narrator1
|
Follow us on