1/13/2016 10:19 AM | |
Joined: 7/9/2015 Last visit: 8/29/2025 Posts: 4443 Rating:
|
Hi,
did you check if all software is compatible? Please check here with compatibility tool: https://support.industry.siemens.com/kompatool/pages/main/index.jsf
You could also start a repair installation of Simatic manager, it could help. Do you have enough free memory on HDD?
Regards, Towome
|
|
|
This contribution was helpful to
1 thankful Users |
1/13/2016 1:01 PM | |
Joined: 5/27/2013 Last visit: 8/12/2024 Posts: 22 Rating:
|
Thanks Towome, I've tried. It said everything's compatible. I've tried to repair the Automation License Manager installation. It got a little bit better, but still a 10min awaiting for SIMATIC Manager to start. Well, I still have space in my HDD. is there any special configuration for the HDD allocation? Regards! |
Last edited by: S7-Tio at: 1/13/2016 1:11:46 PM |
|
1/13/2016 3:08 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello, Have you already seen this, maybe is not your problem but if you want to read..... Step7 5.5 SP4 became slow after installed Tia Portal V13 SP1 |
This contribution was helpful to
1 thankful Users |
1/14/2016 8:34 AM | |
Joined: 5/27/2013 Last visit: 8/12/2024 Posts: 22 Rating:
|
That's exactly what I'm experiencing... after I installed TIA Portal (I don't know about the SP1) my SIMATIC Step7 5.5 became extremely slow to startup. I think the issue here is the ALM or some incompatibility with the licenses... what do you think ? |
1/14/2016 10:44 AM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello S7-Tio, talking to my friends and colleagues about whether the operation of Tia Portal specifically say they have a hard disk SSD as said above from mopS04 and under the requirements of Siemens below and then it would be better a FieldPG with all software preinstalled as I have seen from my colleague who have STEP7 v5.5 and Tia Portal open STEP 7 in 10 seconds or less. You have this requirements? 1) Hardware requirementsYour PC must meet the following minimum requirements for installing STEP 7 Basic / Professional V13:
What are the requirements for installing STEP 7 (TIA Portal ... |
1/28/2016 9:22 AM | |
Joined: 5/27/2013 Last visit: 8/12/2024 Posts: 22 Rating:
|
Hello Ste39, I still couldn't get ahold of a SSD hard-disk to test this, but I guess you're right. My coworkers who have a SSD disk experience a faster load of the SIMATIC Manager. I'll update this entry as soon as I can test with the SSD disk. I guess the problem here is the access to data and not the RAM or Processor performance. Thanks! |