11/2/2016 11:13 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
Hello, which length you need ? For V90 only 2 types available, one for 230V and one for 400V Regards |
This contribution was helpful to
1 thankful Users |
11/2/2016 11:24 AM | ||
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Please refer the attached sheets which will help you to select the power & encoder cable suitable to motor. (Extracts from Siemens manual) Attachment1FL6 motor cable.pdf (475 Downloads) |
|
Last edited by: PISCEAN 2010 at: 11/2/2016 11:27:35 AMLast edited by: PISCEAN 2010 at: 11/2/2016 11:29:29 AM |
||
This contribution was helpful to
1 thankful Users |
11/2/2016 12:15 PM | |
Posts: 1529 Rating:
|
You should download the V90 catalog (obvious search function). See attached. |
This contribution was helpful to
1 thankful Users |
11/2/2016 12:37 PM | |
Joined: 3/12/2015 Last visit: 9/1/2025 Posts: 555 Rating:
|
Hey Christoph, i need the 7m one but when i search for the reference it comes up with a 3m cable even tho the referecne is different that the 3m one, is that just a typo from siemens? Cheers guys for all the answers! |
Last edited by: Jackcaress at: 11/2/2016 12:38:31 PM |
|
11/2/2016 12:46 PM | |
Joined: 1/21/2013 Last visit: 11/20/2024 Posts: 4620 Rating:
|
Hello Jack, From Industry Mall is correct?: Industry Mall - Product Details - Industry Mall - Siemens WW BRAKE CABLE PREASSEMBLED 6FX3002-5BL02 2X0.75, FOR MOTOR S-1FL6 HI 400 WITH V70/V90 MOTION-CONNECT 300 UL/CSA DMAX=6,3MM LENGTH(M) = 7M |
Last edited by: Ste39 at: 11/2/2016 12:47:06 PM |
|
11/2/2016 12:50 PM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
6FX3002-5BL02-1AH0 Length 7 mtr Cable connector motor side 6FX2003-0LL51 HTH |
11/2/2016 1:02 PM | |
Joined: 3/12/2015 Last visit: 9/1/2025 Posts: 555 Rating:
|
Hey guys theres a mistake on the spanish version it says 3m when the same cable in english is 7m |
11/2/2016 1:25 PM | |
Posts: 1529 Rating:
|
Strange.... Did Spain re-define the meter? The Spanish version is correct. I guess I need to keep this in mind when I speak Spanish that 3m in English = 7 meters in Spanish. Does that work equally for Euros to Dollars? This is probably a question best answered by your local contact. |
Last edited by: Jeff Casagrande at: 11/2/2016 1:29:28 PM |
|
11/3/2016 8:24 AM | |
Joined: 3/12/2015 Last visit: 9/1/2025 Posts: 555 Rating:
|
Im not sure if you´re joking lol, spain uses the metric system its just a typo on the website i guess |
Follow us on