(0)| 3/19/2021 3:18 PM | |
|
Posts: 1 Rating:
|
I need some help I have a Siemens A8000 CP-8000 and a Siprotec 5 6MD85 Bay Controller. I want to map the operational values of the relay to 104 IOA adresses on the RTU. I use SICAM WEB and have set PRE3 as 61850 client + server ed. 2 rev 3.16 The IEC 61850 adresses seems to have some attributes errors. - Is it possible to generate a ICD file is the 61850 configurator and upload it to SICAM web and automatically set up all the configuration that has been done in 61850 configurator? Thanks for the help! Regards Nicklas ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/22/2021 09:03:06New subject after splitting |
|
Follow us on