(0)| 2/12/2009 3:30 PM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello Yes that's it.(X3 PE3, D, C -DC link bus module 510 - 650 V) Look at SIMOVERT MASTERDRIVES Vector Control Compendium VC34 (Operating Instructions) (page 23 Configuration example of a single-axis drive of the Compact PLUS type). Look at triangle with Nr.12 (Precharging the capacitor module -When a capacitor module is used, the terminals for precharging the capacitors must be connected.) regards |
Follow us on