(4)| 3/29/2021 9:28 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, In addition of TechnoBlaze his post (very helpful): Consider using the Industry Library V9.0 SP1 (not free). Siemens has integrated some blocks of the former Braumat library into the IL. With it, a block called: BatchIf is added. This blocks lets you create batches from the automation program. You can create a batch / create and release a batch / create, release and start the batch or start the next batch in line. You can configure the block with a recipe name/version, enter Order category, add parameters and materials etc. Maybe this is useful to you? If not, another option is to create batches using the API interface, but this requires programming skill and extra license. Otherwise, you have to stick to the role management... |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on