(1)| 4/6/2021 11:50 PM | |
|
Joined: 9/9/2019 Last visit: 6/9/2025 Posts: 18 Rating:
|
What are those (green tags)? does it can be placed or they just appear? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/07/2021 10:12:37New subject after splitting |
|
| 4/7/2021 1:07 PM | |
|
Posts: 198 Rating:
|
Hello, These are called connectors in the CFC terminology. If no additional line can be drawn due to lack of sheet space, CFC will insert a connector at the block/chart I/O and enter a number in the sheet bar. The corresponding connectors will be assigned the same reference number. Multiple output interconnections that cannot be displayed will be assigned the same reference number. If so many interconnections between sheets are generated that there is insufficient space in the sheet bar for all the entries, an overflow page is created automatically. The overflow page represents an extension of the sheet bars and contains no additional objects. If an output contains multiple interconnections, some of the interconnections may only be displayed as a line. In such an event, a connector is attached to the line. Using this connector technique, you can always display the full CFC structure, regardless of its complexity. For more information - you can refer to section 9.9 Layout of interconnections in CFC Manual. Hope this helps! |
Last edited by: Jen_Moderator at: 04/07/2021 14:18:26Optimized link. |
|
This contribution was helpful to
|
|
| 4/18/2021 1:25 AM | |
|
Joined: 9/9/2019 Last visit: 6/9/2025 Posts: 18 Rating:
|
Thanks so much, that helps me a lot |
Follow us on